AXIS#.HOME.MOVE

Description

AXIS#.HOME.MOVE starts a homing move. AXIS#.OPMODE must be set to 2 (position mode) and AXIS#.CMDSOURCE must be set to 0 (Service).

AXIS#.STOP can be used to stop homing after it has started.


  • When Axis 2 is configured as a gantry (AXIS2.CMDSOURCE = 4), issuing AXIS1.HOME.MOVE starts homing on both Axis 1 and Axis 2. The drive returns an error if AXIS2.HOME.MOVE is commanded.
    To ensure both axes move together during gantry homing, AXIS1.HOME.V, AXIS1.HOME.ACC. and AXIS1.HOME.DEC are used on both axes. The correspoding AXIS2 parameters are ignored.
    When homing completes successfully on both axes, GANTRY.STATE changes to 3, indicating the gantry is active and ready for motion commands.

Versions

Action Version Notes
Implemented 02-00-00-000
Added gantry homing support 02-05-00-000  

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

AXIS#.HOME.MODE

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.HOME.MOVE

6108

17DC

Unsigned8

Read/Write

-

AXIS2.HOME.MOVE

71644

117D

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.MOVE

6108

Unsigned8

Read/Write

-

Related Topics

Homing

Gantry Mode